Mounting - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108

Procedure

  1. Loosen the screws on the front cover and remove the cover (Figure 1).
    Figure 1. Loosen the Cover Screws and Remove the Front Cover

  2. Remove the high-voltage wiring cover at the bottom of the VFD68 Drive (Figure 2).
    Figure 2. Remove the High-Voltage Wiring Cover

Results

Mount the VFD vertically (Figure 1) in an acceptable NEMA-rated enclosure on a non-flammable surface. When you drill mounting holes and mount the VFD, ensure that you do not allow metal chips or other material to enter the VFD housing.

Figure 3. Mounting the VFD68 Drive

See Figure 4 and Table 1 for mounting space requirements.

Figure 4. Required Clearance for Mounting Inside an Enclosure

Table 1. Required Clearance
Dimension 3.7 kW

(5 HP) or Less

5.5–7.5 kW

(7-1/2 to 10 HP)

A 100 mm (4 in.) or more 100 mm (4 in.) or more
B 10 mm (7/16 in.) or more 50 mm (2 in.) or more
C