Selecting a Motor - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108
Important: When selecting the motor, do not exceed the maximum output current rating of the VFD68 Drive.

Motors used with the VFD68Bxx or VFD68Cxx Drive must:

  • be AC induction three-phase motors that are UL Recognized and CSA Certified, or equivalent
  • be rated for: 230 VAC at 50/60 Hz; or 460 VAC at 50/60 Hz
  • have an Inverter Rating (460 VAC motors)
  • have Insulation Class F or better

The VFD68 Drive is intended for use with variable speed motors that are rated for 40:1 operation.

Note: If three-phase power is not available as supply power for the VFD68 Drive, refer to the VFD68 Variable Frequency Drive Technical Bulletin (Part No. 24-7664-3051).