Ordering information - PENN Controls - LIT-125687 - V46 - Pressure Actuated Water Regulating Valve - V46 Low and All-Range Pressure Refrigerant

V46 Pressure-Actuated Water-Regulating Valve Product Bulletin

Brand
PENN Controls
Product name
V46 Low and All-Range Pressure Refrigerant
Document type
Product Bulletin
Document number
LIT-125687
Revision date
2021-08-17
Language
English

When you order water valves, specify the following:

  1. The complete product number.

    If you do not know the product number, determine the following list of information and see Selection charts to select a valve.

    • To determine the valve size that you need, see Selecting the valve size.
    • To determine the refrigerant to use in the system, see Table 4.
      Note: 3/8 in. to 1 1/2 in. valves are supplied with all-range construction. You can use a single valve for either low or high range refrigerants.
    • To determine if you need a standard open high valve, see Table 1.
    • If you need a valve with a bronze body and MONEL internal parts, you need a Navy or maritime service valve.
  2. To determine the companion flange kit by part number, see Companion flanges and gaskets.
  3. If you need a mounting bracket for 3/8 in. and 1/2 in. valve sizes only, to determine its position on the valve, see Options.