Two-Speed Fan Motor Control Using Any Compatible Pressure, Humidity, or Temperature Sensor Application Note - PENN Controls - LIT-1900712 - C450CCN - C450YNN - Bulb controller - C450CCN Standard Control Module Two Relay Outputs - C450YNN‐1 Power Module
- Brand
- PENN Controls
- Product name
- C450CCN Standard Control Module Two Relay Outputs
- C450YNN‐1 Power Module
- Document type
- Application Note
- Document number
- LIT-1900712
- Revision date
- 2020-04-15
- Language
- English