Description - PENN Controls - LIT-1922255 - T22BBC - T22ABC - T22AAA - T25A - T26A - T22SDA - T22SEB - T22TFB - T22SFB - T26J - T22JAA - T22JCC - T26T - T26S - T22CBC - Line-Voltage Thermostat - T25 Line‐Voltage Thermostat - T26 Line‐Voltage Thermostat - T22 Line‐Voltage Thermostat

T22, T25, and T26 Series Line Voltage Wall Thermostat for Heating and Cooling Catalog Page

Product
Document type
Catalog Page
Document number
LIT-1922255
Revision date
2021-09-29

Use the T22, T25, and T26 Series for line voltage control of residential, commercial, or industrial heating or year-round air conditioning. You do not require heat or cold anticipators. The liquid-charged temperature sensing element and highly efficient diaphragm and leverage provide close temperature control.

Refer to the following documents for important product application information:

  • T22 Series Line Voltage Thermostats with Selector Switch Product Bulletin (LIT-125630)
  • T25 Two-Stage Room Thermostat Product Bulletin (LIT-125640)
  • T26 Series Line Voltage Thermostats Product Bulletin (LIT-125645)
Figure 1. T26 Series Line Voltage Wall Thermostat