Contact information - PENN Controls - LIT-1900864 - C450CCN - C450SBN - C450YNN - System 450 Multi-Purpose Modular Control System - C450CCN Standard Control Module Two Relay Outputs - C450SBN Expansion Module One Relay Output - C450YNN‐1 Power Module

Solar Heating Control Applications with Differential Temperature Control Application Note

Product name
C450CCN Standard Control Module Two Relay Outputs
C450SBN Expansion Module One Relay Output
C450YNN‐1 Power Module
Document type
Application Note
Document number
LIT-1900864
Revision date
2020-04-14