Solar Heating Control Applications with Differential Temperature Control Application Note - PENN Controls - LIT-1900864 - C450CCN - C450SBN - C450YNN - Communication control module - C450CCN Standard Control Module Two Relay Outputs - C450SBN Expansion Module One Relay Output - C450YNN‐1 Power Module
- Brand
- PENN Controls
- Product name
- C450CCN Standard Control Module Two Relay Outputs
- C450SBN Expansion Module One Relay Output
- C450YNN‐1 Power Module
- Document type
- Application Note
- Document number
- LIT-1900864
- Revision date
- 2020-04-14
- Language
- English