Description - PENN Controls - LIT-1927340 - V47 - V46 - V48 - Temperature Actuated Water Regulating Valve - Pressure Actuated Water Regulating Valve - V47 Temperature Actuated Water Regulating Valve - V48 Low and All‐Range Pressure Refrigerant - V46 Low and All‐Range Pressure Refrigerant

STT Water Valve Renewal Kit for V46, V47, and V48 Series Valves Catalog Page

Product
Valves and Actuators > Water Valves > V47 Temperature Actuated Water Regulating Valve
Document number
LIT-1927340
Revision date
2020-04-22

These renewal kits include a seat, disc, diaphragms, and all additional internal parts required to recondition the valves.

WARNING
  • Risk
  • This product is made of copper alloy, which contains lead. The product is therefore not to be used on drinking water.