Room Temperature, Humidity, and Static Pressure Control System with Communications Application Note - PENN Controls - LIT-1900879 - C450CEN - C450SBN - C450SCN - C450SQN - Communication control module - C450CEN Communications Control Module for Ethernet - C450SBN Expansion Module One Relay Output - C450SCN Expansion Module Two Relay Outputs - C450SQN Expansion Module Two Analog Outputs

Brand
PENN Controls
Product name
C450CEN Communications Control Module for Ethernet
C450SBN Expansion Module One Relay Output
C450SCN Expansion Module Two Relay Outputs
C450SQN Expansion Module Two Analog Outputs
Document type
Application Note
Document number
LIT-1900879
Revision date
2020-04-14
Language
English