Installing and commissioning the temperature sensors - PENN Controls - LIT-12013314 - RMZ1214R10-EU - RMZ-1214-E10 - RMZ1218C10-UK - RMZ1214E61-DS1 - RMZ1218C40-US - RMZ1218C10-EU - RMZ1214E11-NT3 - RMZ1214E11-NT1 - RMZ1214R10-US - RMZ1218C40-UK - RMZ1214E20 - PC10 - RMZ1214R10-UK - RMZ1218C40-EU - RMZ1218C10-US - PENN Connected - PENN Connected PC10

PENN Connected PC10 Install and Commissioning Guide

Product
Refrigeration > Gateways > PENN Connected PC10
Building Automation Systems > Building Automation Systems > PENN Connected PC10
Network and Communications > Gateways and Routers > PENN Connected PC10
Document number
LIT-12013314
Revision date
2021-08-25

Procedure

  1. To power on the sensor, swipe it once from top to bottom with a magnet. The following light sequence indicates connection to the network:
    • Sensor light turns blue
    • Sensor light flashes green approximately 4 times
    • Sensor light turns off
  2. Mount the sensor with or without a bracket in the refrigeration unit. Secure the sensor with screws, tie-wraps, or double-sided tape.
  3. Attach a sticker to a visible location on the refrigeration unit.
  4. On the Android device, in the upper-right of the Penn Commissioner app, tap +.
  5. Commission a sensor in one of the following ways:
    • Tap SCAN to open the camera. Scan the QR code or the barcode located on the side of the sensor.
    • In the Or Enter Device MAC Address field, enter the unique 16-digit serial number located on the side of the sensor.
  6. Follow the remaining on-screen instructions and enter the required data for each sensor; you can then view the temperature and the received signal strength indication (RSSI) for each sensor.
    Note: To change the alarm parameters, go to the PENN Connected desktop platform and, on the Manage Alarms screen, click on the alarm row to open the Edit Sensor dialog box.

Results

When you complete the commissioning process, the sensor name displays in green on the app. To commission another sensor, repeat the procedure.