Repeaters - PENN Controls - LIT-12013314 - PC10 - RMZ-1214-E10 - RMZ1214E11-NT1 - RMZ1214E11-NT3 - RMZ1214E20 - RMZ1214E61-DS1 - RMZ1214R10-EU - RMZ1214R10-UK - RMZ1214R10-US - RMZ1218C10-EU - RMZ1218C10-UK - RMZ1218C10-US - RMZ1218C40-EU - RMZ1218C40-UK - RMZ1218C40-US - PENN Connected - PENN Connected PC10

PENN Connected PC10 Install and Commissioning Guide

Product
Refrigeration > Gateways > PENN Connected PC10
Building Automation Systems > Building Automation Systems > PENN Connected PC10
Network and Communications > Gateways and Routers > PENN Connected PC10
Document type
Commissioning Guide
Document number
LIT-12013314
Revision date
2021-08-25

The repeaters extend the range of the wireless network. The maximum range of a repeater is 25 m (82 ft) within a line of sight of the gateway.

Plug the repeaters into a dedicated mains power supply socket; each repeater includes a local power adapter. Each repeater can connect to 15 sensors. The repeaters do not require commissioning. See the following figure for an example of an installation location for repeaters.

Figure 1. A repeater in position on top of a cabinet