Procedure
- Install the gateway at a central point of the premises, and at a height that prevents interference from staff and customers. See Gateway for more information.
- Secure the gateway with screws, tie-wraps, or double-sided tape. You can also use an open enclosure.
- Connect the gateway to a power supply, and move the antenna into a vertical position.
-
Check that the gateway powers on in the following light
sequence:
- Blue network light blinks rapidly to indicate connection to the ZigBee network
- Red data light blinks to indicate the transmission of data through the GSM network
- Green server light remains steady to indicate connection to the internet
Figure 1. Gateway light sequence
Callout Description 1 Blue network light 2 Red data light 3 Green server light - On the Android device, open the PENN Commissioner app, and enter the username and password that the PENN Connected administrator sent by email.
-
Commission the gateway in one of the following ways:
- In the ICCID or IMEI field, enter the unique 15 or 16 digit number located on the side of the gateway, and tap Register.
- Tap SCAN GATEWAY to open the camera. Scan the QR code or the barcode located on the side of the gateway, and tap Register.
When registered, in the upper-right of the app, you can tap the signal bars to view the GSM signal strength.