Installing and commissioning the door sensors - PENN Controls - LIT-12013314 - RMZ1214R10-EU - RMZ-1214-E10 - RMZ1218C10-UK - RMZ1214E61-DS1 - RMZ1218C40-US - RMZ1218C10-EU - RMZ1214E11-NT3 - RMZ1214E11-NT1 - RMZ1214R10-US - RMZ1218C40-UK - RMZ1214E20 - PC10 - RMZ1214R10-UK - RMZ1218C40-EU - RMZ1218C10-US - PENN Connected - PENN Connected PC10

PENN Connected PC10 Install and Commissioning Guide

Product
Refrigeration > Gateways > PENN Connected PC10
Building Automation Systems > Building Automation Systems > PENN Connected PC10
Network and Communications > Gateways and Routers > PENN Connected PC10
Document number
LIT-12013314
Revision date
2021-08-25

Procedure

  1. To power on the sensor, swipe it once from top to bottom with a magnet. The following light sequence indicates connection to the network:
    • Sensor light turns blue
    • Sensor light flashes green approximately 4 times
    • Sensor light turns off
  2. On the Android device, in the upper-right of the PENN Commissioner app, tap +.
  3. Commission a sensor in one of the following ways:
    • Tap SCAN to open the camera. Scan the QR code or the barcode located on the side of the sensor.
    • In the Or Enter Device MAC Address field, enter the unique 16-digit serial number located on the side of the sensor.
  4. Follow the remaining on-screen instructions and enter the required data for each sensor.
  5. Mount the sensor with or without a bracket near the chiller or freezer room door. Secure the sensor with screws, tie-wraps, or double-sided tape.
    Note: If the door sensor is more than 25 m from the gateway, install another repeater nearby.
  6. Attach the magnet and reed strip to the frame of the chiller or freezer room door with a maximum gap of 20 mm.
  7. Attach a sticker to a visible location on the refrigeration unit.