Procedure
-
To power on the sensor, swipe it once from top to bottom with a
magnet. The following light sequence indicates connection to the network:
- Sensor light turns blue
- Sensor light flashes green approximately 4 times
- Sensor light turns off
- On the Android device, in the upper-right of the PENN Commissioner app, tap +.
-
Commission a sensor in one of the following ways:
- Tap SCAN to open the camera. Scan the QR code or the barcode located on the side of the sensor.
- In the Or Enter Device MAC Address field, enter the unique 16-digit serial number located on the side of the sensor.
- Follow the remaining on-screen instructions and enter the required data for each sensor.
-
Mount the sensor with or without a bracket near the chiller or
freezer room door. Secure the sensor with screws, tie-wraps, or double-sided
tape.
Note: If the door sensor is more than 25 m from the gateway, install another repeater nearby.
- Attach the magnet and reed strip to the frame of the chiller or freezer room door with a maximum gap of 20 mm.
- Attach a sticker to a visible location on the refrigeration unit.