Wiring - PENN Controls - LIT-121445 - P67AA - P67CA - Electromechanical Pressure Control - P67 Low Pressure Control

P67 Series Low Range Pressure Control Technical Bulletin

Product
Controls > Pressure Controls > P67 Low Pressure Control
Document number
LIT-121445
Document revision
Revision date
2023-02-20
Product status
Active
docpartnumberlabel
Part No.
Part number
A16381YFLY
CAUTION
  • Risk of electric shock
  • Disconnect power supply before wiring connections are made to avoid possible electrical shock or damage to equipment.
CAUTION
  • Risk
  • Use the supplied terminal screws in the switch (#8/32 x 1/4 in.). Longer terminal screws can interfere with the switch mechanism and damage the switch.

The control comes with large, coded, screw-type terminals for simplified installation.

Make all wiring connections using copper conductors only, and in accordance with the National Electrical Code or local regulations. Electrical loads exceeding the rating of the control should be controlled by means of an intermediate relay or starter.