Mounting - PENN Controls - LIT-121445 - P67AA - P67CA - Electromechanical Pressure Control - P67 Low Pressure Control

P67 Series Low Range Pressure Control Technical Bulletin

Product
Controls > Pressure Controls > P67 Low Pressure Control
Document type
Technical Bulletin
Document number
LIT-121445
Document revision
Revision date
2023-02-20
Product status
Active
docpartnumberlabel
Part No.
Part number
A16381YFLY

Mount the pressure control in any position in an area that is protected from the weather. For support, you can secure the enclosure to an adjoining surface either directly, or with the mounting bracket provided. Models with barbed fitting are for use with 1/4 in. O.D. polytubing.