General description - PENN Controls - LIT-121445 - P67AA - P67CA - Electromechanical Pressure Control - P67 Low Pressure Control

P67 Series Low Range Pressure Control Technical Bulletin

Product
Controls > Pressure Controls > P67 Low Pressure Control
Document number
LIT-121445
Document revision
Revision date
2023-02-20
Product status
Active
docpartnumberlabel
Part No.
Part number
A16381YFLY

Easily adjust the operating point of the control, as well as the differential, with the externally located adjustment screws on the top of the control enclosure. Both the cut-in and cutout control set points are quick to read on the large graduated scale on the front of the case.

The pressure control features a non-metallic diaphragm member which moves in response to changes in air pressure. As a result, the lever-mechanism diaphragm actuates a heavy duty electrical contact.