Application - PENN Controls - LIT-121445 - P67AA - P67CA - Electromechanical Pressure Control - P67 Low Pressure Control

P67 Series Low Range Pressure Control Technical Bulletin

Product
Controls > Pressure Controls > P67 Low Pressure Control
Document number
LIT-121445
Document revision
Revision date
2023-02-20
Product status
Active
docpartnumberlabel
Part No.
Part number
A16381YFLY
Figure 1. P67 Pressure Control with barbed fitting

Use the P67 Pressure Control when it is necessary to close or open an electrical circuit on the basis of a predetermined air pressure signal. Applications include the control of air compressors, fans, pilot lights, and resistance heating elements.

Important: Use the P67 Series Low Range Pressure Control only as an operating control. Where failure or malfunction of the P67 Low Range Pressure Control could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the P67 Low Range Pressure Control.