Wiring - PENN Controls - LIT-12013896 - P597 - Pressure Transducer - P597 Electronic Pressure Transducer

P597 Series Electronic Pressure Transducers Product Bulletin

Product
Switches and Electrical > Pressure Transducers > P597 Electronic Pressure Transducer
Document number
LIT-12013896
Revision date
2023-04-07
Important:
  • Ensure that all wiring conforms to the regional, national, and local electrical codes and regulations.
  • Do not exceed the transducer's electrical ratings. See Table 1.
  • Do not extend the wiring harness leads more than 76 m (250 ft). Use 22 AWG stranded, twisted, 3-wire, shielded cable to extend the wiring harness leads.
  • Do not run low-voltage cable in conduit or wiring troughs with high-voltage wires.
  • Ensure that the shielded cable is terminated according to code and the control’s instructions.

Additionally, observe the following warning when you wire or service a P597 transducer in a hazardous location.

WARNING
  • Risk of Explosion or Fire.
  • Do not disconnect the P597 Series Electronic Pressure Transducer while its circuit is energized, unless the area is known to be nonhazardous. Disconnecting the P597 Transducer in a hazardous area while its electrical circuit is energized may result in an explosion or fire, and may cause serious injury or death.
Avertissement
  • Risque de explosion ou incendie
  • Ne pas déconnecter le P597 Series Electronic Pressure Transducer lorsque son circuit est sous tension, sauf s'il est avéré que la zone est non dangereuse. La déconnexion du P597 Transducer dans une zone dangereuse alors que son circuit électrique est sous tension risque d'entraîner une explosion ou un incendie et de provoquer des blessures graves, voire mortelles.