Mounting with braze connections - PENN Controls - LIT-12013896 - P597 - Pressure Transducer - P597 Electronic Pressure Transducer

P597 Series Electronic Pressure Transducers Product Bulletin

Product
Switches and Electrical > Pressure Transducers > P597 Electronic Pressure Transducer
Document number
LIT-12013896
Revision date
2023-04-07

To mount the transducer with braze connections, complete the following steps:

Procedure

  1. Check the heat in the location that you plan to mount the transducer. To avoid damage to the transducer, ensure that the copper tube or fitting receives all of the heat, and that it heats only by conduction. Do not exceed 135°C (275°F) where the copper tube meets the P597 body.
  2. Wrap the transducer end of the copper tube with a quenching cloth for added protection.