Mounting - PENN Controls - LIT-12013896 - P597 - Pressure Transducer - P597 Electronic Pressure Transducer

P597 Series Electronic Pressure Transducers Product Bulletin

Product
Switches and Electrical > Pressure Transducers > P597 Electronic Pressure Transducer
Document number
LIT-12013896
Revision date
2023-04-07
NOTICE
  • Risk of Property Damage
  • Mount the pressure control separately from the electrical cabinet and seal all electrical piping to prevent ammonia from migrating to electrical components. Where there may be exposure to ammonia, use only ammonia-compatible control modules and pressure connections. System shutdown due to improper adjustment may cause property damage.
AVIS
  • Risque de dégâts matériels
  • Installer le régulateur de pression séparément de l'armoire électrique et étanchéifier tous les conduits électriques afin d'éviter que de l'ammoniac n'entre en contact avec des composants électriques. En cas d'exposition potentielle à de l'ammoniac, utiliser uniquement des modules de régulation et des raccords de pression compatibles avec la présence d'ammoniac.- L'arrêt du système en raison d'un réglage inapproprié risque de provoquer des dégâts matériels.
Important:
  • When you install the P597 transducers, observe all regulations governing the handling and containment of hazardous or regulated materials such as refrigerants or lubricants.
  • Locate pressure tap points on the top side of the refrigerant lines to reduce risk of equipment damage or malfunction caused by accumulation of oil, liquids, or sediment at the transducer-to-refrigeration port pressure connection.
  • Position the transducer away from the compressor discharge to avoid severe pressure pulsations on high-side pressure connections.