P499 transducers are UL recognized for use in Class I, Division 2 hazardous locations. Follow these additional guidelines when wiring or servicing a P499 transducer in a hazardous location.
- P499 Series Pressure Transducer models do not have provisions for field wiring. They are suitable for factory installation only. P499 transducers must be installed in a suitable enclosure.
WARNING
Avertissement
Figure 1 shows the wire designations for a P499 transducer used in 0.5 VDC to 4.5 VDC and 0 VDC to 10 VDC applications.
Figure 1. Wire designations for 0.5 VDC to 4.5 VDC and 0 VDC to 10 VDC transducer applications

Figure 2 shows the wire designations for a P499 transducer used in 4 mA to 20 mA applications.
Figure 2. Wire designations for 4 mA to 20 mA transducer applications

Figure 3 shows the wire colors for the wire terminations in the Packard connector plug.
Figure 3. Wire terminations by wire color at Packard connector plug on wire harness

Figure 4 show the pins in the Packard connector socket on the P499 transducer and the associated wire color the pins are connected to when the Packard connector plug is connected to the socket.
Figure 4. Pin terminations at P499 Packard connector socket by wire color