About this task
CAUTION
ATTENTION
Important:
- When installing the P499 transducers, observe all regulations governing the handling and containment of hazardous or regulated materials (refrigerants or lubricants).
- Locate pressure tap points on the top side of the refrigerant lines to reduce risk of equipment damage or malfunction caused by accumulation of oil, liquids, or sediment in the pressure chamber.
- Avoid severe pressure pulsations on high-side pressure connections by positioning the transducer away from compressor discharge.
Procedure
To mount the P499 transducer:
- Hand thread the P499 transducer to the pressure tap point.
- Tighten the connection using the wrench flats provided to avoid damaging the transducer.
- Perform a leak test on fittings and connections before putting the system into operation.