Operation - PENN Controls - P10BJ - Electromechanical Pressure Control - P10 Low Pressure Control

P10BJ Low Pressure Control Installation Guide

Product
Controls > Pressure Controls > P10 Low Pressure Control
Document type
Installation Guide
Document revision
Revision date
2023-12-20
Product status
Active
Part number
A163829H9B

The control has a snap-acting single-pole, double-throw (SPDT) switch for slow or fast-cycling applications. A calibrated indicator scale indicates the high setting of the control.

Figure 1. Terminal switch operation on a pressure increase for the P10BJ SPDT model

On a rise in pressure, the contacts from red (R) to blue (B) open, and simultaneously the contacts from red to yellow (Y) close.