Wiring - PENN Controls - P10BJ - Electromechanical Pressure Control - P10 Low Pressure Control

P10BJ Low Pressure Control Installation Guide

Product
Controls > Pressure Controls > P10 Low Pressure Control
Document type
Installation Guide
Document revision
Revision date
2023-12-20
Product status
Active
Part number
A163829H9B
WARNING
  • Risk of electrical shock.
  • Disconnect the power supply before wiring connections are made to avoid possible electrical shock.
CAUTION
  • Risk of equipment damage.
  • Disconnect the power supply before wiring connections are made to avoid damage to the equipment.
Important: Use the supplied 8-32 x 1/4 in. binder head terminal screws in the switch. Substitution of other screws could cause problems in making correct connections.

Use only copper conductors to make all wiring connections. Wire the control in accordance with the local, national, and regional regulations.

The terminals on SPDT models are color-coded. The common terminal is red. The red to yellow terminals open on a drop in pressure. The red to blue terminals close on a drop in pressure. See Figure 1.