Adjusting the set point - PENN Controls - P10BJ - Electromechanical Pressure Control - P10 Low Pressure Control

P10BJ Low Pressure Control Installation Guide

Product
Controls > Pressure Controls > P10 Low Pressure Control
Document type
Installation Guide
Document revision
Revision date
2023-12-20
Product status
Active
Part number
A163829H9B

Procedure

  1. Connect an air pressure gauge and a variable pressure source to the control's air connector.
  2. Turn the set point adjusting screw so that the indicator is at the pressure setting that you want.
  3. Apply and gradually increase the air pressure. Note the pressure at which the contacts transfer.
  4. Remove the air pressure and slightly turn the set point adjusting screw.
  5. Repeat the steps of applying pressure, noting the switching pressure, and making adjustments, until the switch occurs at the pressure setting that you want.