Applications - PENN Controls - P10BJ - Electromechanical Pressure Control - P10 Low Pressure Control

P10BJ Low Pressure Control Installation Guide

Product
Controls > Pressure Controls > P10 Low Pressure Control
Document revision
Revision date
2023-12-20
Product status
Active
Part number
A163829H9B
Figure 1. Interior view of the single-stage P10BJ pressure control

The P10BJ Low Pressure Controls are designed for applications that use a pneumatic air signal to operate an electric or electronic device. Other applications include the control of pumps and small air compressors.

Important: Use the P10BJ low pressure control only as an operating control. Where failure or malfunction of the control could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the control.