Ordering information - PENN Controls - LIT-125400 - P10FC - P10BG - P10BC - P10PA - Electromechanical Pressure Control - P10 Low Pressure Control

P10 Series Low Range Pressure Control Product Bulletin

Product
Controls > Pressure Controls > P10 Low Pressure Control
Document number
LIT-125400
Revision date
2023-12-20
Product status
Active

To order, specify the following requirements:

  • Model type number
  • Range
  • Optional constructions
  • Control setting and differential, if other than standard. If you need a two-stage model, specify the following requirements:
    • High stage operating set point
    • Low stage operating set point
    • Switch differential
    • Between-stage differential