Applications - PENN Controls - LIT-125400 - P10FC - P10BG - P10BC - P10PA - Electromechanical Pressure Control - P10 Low Pressure Control

P10 Series Low Range Pressure Control Product Bulletin

Product
Controls > Pressure Controls > P10 Low Pressure Control
Document number
LIT-125400
Revision date
2023-12-20
Product status
Active
Figure 1. Single-stage P10 pressure control with barbed fitting and mounting bracket
Figure 2. Two-stage pressure control

The P10 Series Low Pressure Controls are for applications that use a pneumatic air signal to operate an electric or electronic device, including the following applications:

  • Pressure-electric switches in pneumatic systems
  • Control of pumps or small air compressors
  • Pressure-electric interlock of fluid flow systems
Important: Use the P10 low pressure control only as an operating control. Where failure or malfunction of the control could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the control.