Adjusting the set point - PENN Controls - P10BC - P10BG - P10FC - P10PA - Electromechanical Pressure Control - P10 Low Pressure Control
P10 Series Low Pressure Control Installation Guide
- Product
- Controls > Pressure Controls > P10 Low Pressure Control
- Document type
- Installation Guide
- Document revision
- J
- Revision date
- 2023-12-20
- Product status
- Active
- Part number
- 997-437
Procedure
-
Connect an air pressure gauge and a variable pressure source to the control's
air connector.
-
Turn the set point adjusting screw so that the indicator is at the pressure
setting that you want.
-
Apply and gradually increase the air pressure. Note the pressure at which the
contacts transfer.
-
Remove the air pressure and slightly turn the set point adjusting screw.
-
Repeat the steps of applying pressure, noting the switching pressure, and
making adjustments, until the switch occurs at the pressure setting that you
want.