Wiring - PENN Controls - P100AC - P100AP - P100CC - P100CP - P100DA - Electromechanical Pressure Control - P‐Series Encapsulated Pressure Switch

P-Series Encapsulated Pressure Controls Installation Guide

Product
Document type
Installation Guide
Document revision
A
Revision date
2019-08-08
docpartnumberlabel
Part No.
Part number
24-7664-3337
WARNING
  • Risk of Electric Shock.
  • Disconnect the power supply before making electrical connections. Contact with components carrying hazardous voltage can cause electric shock and may result in severe personal injury or death.
Avertissement
  • Risque de décharge électrique.
  • Débrancher l'alimentation avant de réaliser tout branchement électrique. Tout contact avec des composants conducteurs de tensions dangereuses risque d'entraîner une décharge électrique et de provoquer des blessures graves, voire mortelles.
Figure 1. P-Series Control Wiring

Important: Make all wiring connections in accordance with National Electrical Code and all local regulations. Use copper conductors only. Do not exceed the control’s electrical rating.

Standard P-Series controls are available with several electrical switch options. Refer to the P-Series Encapsulated Pressure Controls Product Bulletin, LIT-12013066 for model-specific switch action, wiring information, and electrical ratings.