Electrical Ratings - PENN Controls - P100AC - P100AP - P100CC - P100CP - P100DA - Electromechanical Pressure Control - P‐Series Encapsulated Pressure Switch

P-Series Encapsulated Pressure Controls Installation Guide

Product
Document type
Installation Guide
Document revision
A
Revision date
2019-08-08
docpartnumberlabel
Part No.
Part number
24-7664-3337
General Silver Contact Ratings PS Models PM Models PR Models1 PC Models1
28 VDC Resistive 2 A n/a 3 A 15 A
24 VAC Pilot Duty 125 VA n/a 125 VA 125 VA
120 VAC Pilot Duty 375 VA 375 VA 375 VA 480 VA
240 VAC Pilot Duty 375 VA 375 VA 375 VA 720 VA
277 VAC Pilot Duty n/a n/a 375 VA 720 VA
120 VAC Inductive 5.8 FLA 5.8 FLA 6 FLA 13 FLA
34.8 LRA 34.8 LRA 40.2 LRA 65 LRA
240 VAC Inductive 2.9 FLA 2.9 FLA 4 FLA 10 FLA
17.4 LRA 15 LRA 26.4 LRA 45 LRA
277 VAC Inductive n/a n/a 4 FLA 10 FLA
n/a n/a 26.4 LRA 45 LRA
480 VAC Inductive n/a n/a n/a 4 FLA
n/a n/a n/a 24 LRA
480 VAC Inductive n/a n/a n/a 3.2 FLA
n/a n/a n/a 20 LRA

Gold Plated Contacts - Dry Circuit Rating: 400 mA at 12 VAC maximum, non-arcing loads.

Note: If the Dry Circuit Rating is exceeded, the Dry Circuit Rating is rendered invalid and only the Silver Contacts General Ratings apply to the switch contacts.
1 For single-pole, double-throw (SPDT) switches, only one contact pair (COM to NO or COM to NC) can be used at the specified inductive rating, the other contact pair must be used at the pilot duty rating.