Description - PENN Controls - LIT-1900004 - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - MS3 Multi‐Stage Temperature Controller - MS1 One-Stage Temperature Controller - MS4 Multi‐Stage Temperature Controller

MS Series Temperature Stage Control Modules Catalog Page

Product
Controls > Temperature Controls > MS1 One-Stage Temperature Controller
Document type
Catalog Page
Document number
LIT-1900004
Revision date
2020-04-22

The MS Series Temperature Controls are versatile, microprocessor-based, multifunction, programmable temperature controls. They are designed for single and multiple-stage temperature control applications.

Depending on the model selected, the MS Series Controls can operate in the following modes:

  • Direct mode
  • Reverse mode
  • Deadband mode
  • Independent Setpoint mode

The MS Series Controls have large, easy-to-read, red LED displays. These compact controls are available in panel mount and DIN rail mount models. MS Series Controls use the A99B temperature sensors, which allow remote mounting of the display unit.

Refer to the MS Series Multi-Stage Electronic Temperature Controls Product Bulletin (LIT-125198) for important product application information.

Figure 1. MS4 Series Panel and DIN Rail Mount, Multi-Stage, Electronic Temperature Controls