System setup parameters - PENN Controls - LIT-12013106 - MR534AFDN - MR534AFDV - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - MR5xx Panel‐Mount Refrigeration and Defrost Controller

MR5 Series Panel Mount Case Controller Product Bulletin

Brand
PENN Controls
Product name
MR5xx Panel‐Mount Refrigeration and Defrost Controller
Document type
Product Bulletin
Document number
LIT-12013106
Revision date
2019-10-08
Product status
Discontinued
Language
English

The System Setup parameters define the system attributes, hardware features, and hard-wired components of the refrigeration system. The MR5 Controller includes the following system setup parameters:

  • Time and date
  • Defrost type
  • Defrost termination type
  • Evaporator fan type
  • Sensor type
  • Units of temperature in Celsius or Fahrenheit
  • LCD brightness
  • System name