Refrigeration mode - PENN Controls - LIT-12013106 - MR534AFDN - MR534AFDV - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - MR5xx Panel‐Mount Refrigeration and Defrost Controller

MR5 Series Panel Mount Case Controller Product Bulletin

Product
Document type
Product Bulletin
Document number
LIT-12013106
Revision date
2019-10-08
Product status
Discontinued

Refrigeration mode is the normal operating mode of the MR5 Controller. The system cycles the compressor on and off, and operates the evaporator fans according to the setup selections to maintain the setpoint temperature in the refrigerated space. While in refrigeration mode, the Fan icon indicates the evaporator fan relay status and the defrost relay and Defrost icon remain off. The LCD UI displays the HOME screen, which shows the system name, date, time, space temperature, and setpoint.