Binary inputs and alarms - PENN Controls - LIT-12013106 - MR534AFDN - MR534AFDV - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - MR5xx Panel‐Mount Refrigeration and Defrost Controller

MR5 Series Panel Mount Case Controller Product Bulletin

Brand
PENN Controls
Product name
MR5xx Panel‐Mount Refrigeration and Defrost Controller
Document type
Product Bulletin
Document number
LIT-12013106
Revision date
2019-10-08
Product status
Discontinued
Language
English

The MR5 Controller includes the following binary inputs and alarms:

  • The BI1 and BI2 binary inputs interface monitors binary and analog signals, and defines conditions and actions based on those signals. The binary inputs receive signals from a door switch or a refrigerant leak detector. When the MR5 Controller receives a signal, the system performs a specific action, such as sounding an alarm.
  • Cooling shutdown occurs when one of the two binary input modes receives an external signal. When the system receives an external signal, the MR5 Controller turns the compressor and fan off.
  • System shutdown takes priority over the normal control of the compressor, defrost, and fan relays. System shutdowns occur during an alarm condition, such as a refrigerant leak.