Observe the following MR5 Controller location and mounting guidelines:
- Mount the controller on a flat, even surface.
- Make sure the mounting surface can support the controller assembly, mounting hardware, and any user-supplied panel or enclosure.
- Make sure the controller is in the proper orientation for easy wiring, setup, and viewing.
- Allow sufficient space to connect and route wires, view the LCD, and use the touch pad.
- Identify the appropriate mounting hardware.
- Mount the controller in locations free from corrosive vapors, and observe all ambient operating conditions.
- Do not mount the controller on surfaces that vibrate.
- Do not mount the controller in a location where high-voltage relays, motor starters, other sources of electromagnetic emissions, and strong radio frequency may cause electromagnetic interference (EMI).
- Do not install the controller in airtight enclosures.
- Do not install heat-generating devices that may cause the ambient temperature to exceed 60°C (140°F) in an enclosure with the controller.