Mounting the controller - PENN Controls - MR534AFDN - MR534AFDV - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - MR5xx Panel‐Mount Refrigeration and Defrost Controller

MR5 Series Panel Mount Case Controller Installation Guide

Product
Document revision
D
Revision date
2019-08-16
Product status
Discontinued
Part number
24-07664-03388

About this task

The following figures show how to mount the controller to a panel.

Procedure

  1. Cut an opening using the dimensions shown in the following figure:


  2. Slide the controller into the panel opening, until the gasket is pressed firmly against the panel.


  3. To affix the controller to the panel, slide the clips along the edge of the controller.