Software terms - PENN Controls - LIT-1900699 - A99 - C450YNN - C450CCN - C450SCN - System 450 Multi-Purpose Modular Control System - C450YNN‐1 Power Module - A99 Temperature Sensor - C450SCN Expansion Module Two Relay Outputs - C450CCN Standard Control Module Two Relay Outputs

Heating and Cooling Control with System Status Indication Application Note

Product
Controls > Multi-Purpose Modular Controls > C450SCN Expansion Module Two Relay Outputs
Sensors and Meters > Temperature Sensors > A99 Temperature Sensor
Controls > Multi-Purpose Modular Controls > C450CCN Standard Control Module Two Relay Outputs
Document type
Application Note
Document number
LIT-1900699
Revision date
2020-04-15

Use of the software that is in (or constitutes) this product, or access to the cloud, or hosted services applicable to this product, if any, is subject to applicable terms set forth at www.johnsoncontrols.com/techterms. Your use of this product constitutes an agreement to such terms.