Cooling Tower Control with Two-Speed Fan/Low Temperature Lockout Application Note - PENN Controls - LIT-1900637 - C450CBN - C450SCN - C450YNN - Bulb controller - C450CBN Standard Control Module One Relay Output - C450SCN Expansion Module Two Relay Outputs - C450YNN‐1 Power Module
- Brand
- PENN Controls
- Product name
- C450CBN Standard Control Module One Relay Output
- C450SCN Expansion Module Two Relay Outputs
- C450YNN‐1 Power Module
- Document type
- Application Note
- Document number
- LIT-1900637
- Revision date
- 2020-04-15
- Language
- English