Setting a new device address - PENN Controls - ADPT-MR5-RS485 - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - ADPT‐RS285‐MR5 Communications Adapter

ADPT-MR5-RS485 Network Communications Adapter Installation Guide

Product
Document revision
A
Revision date
2019-07-11
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-07664-03450

About this task

The default BACnet device address is "07" and the default device ID is "1". To set a unique network device address for the controller and adapter, complete the following steps:

Procedure

  1. On the HOME screen, press and hold MENU/ESC for 2 seconds to go to the STATUS start screen.
  2. Press DOWN to go to the SYSTEM SETUP start screen, and press SET.
  3. Press DOWN to go to the BACNET start screen and press SET.
  4. On the DEVICE ADDRESS screen, press SET to set a new device address.