Connecting the adapter and cable - PENN Controls - ADPT-MR5-RS485 - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - ADPT‐RS285‐MR5 Communications Adapter
ADPT-MR5-RS485 Network Communications Adapter Installation Guide
- Product
- Document revision
- A
- Revision date
- 2019-07-11
- Product status
- Discontinued
- docpartnumberlabel
- Part No.
- Part number
- 24-07664-03450
Procedure
-
Slide the adapter along the track at the side of the controller as shown in the
following figure until the adapter fits against the end of the clip.
Figure 1. Connecting the adapter
-
Press the cable's 10-pin connector into the communications connector on the
controller as shown in the following figure.
Figure 2. Connecting the lead