Connecting the adapter and cable - PENN Controls - ADPT-MR5-RS485 - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - ADPT‐RS285‐MR5 Communications Adapter

ADPT-MR5-RS485 Network Communications Adapter Installation Guide

Product
Document type
Installation Guide
Document revision
A
Revision date
2019-07-11
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-07664-03450

Procedure

  1. Slide the adapter along the track at the side of the controller as shown in the following figure until the adapter fits against the end of the clip.
    Figure 1. Connecting the adapter

  2. Press the cable's 10-pin connector into the communications connector on the controller as shown in the following figure.
    Figure 2. Connecting the lead