CAUTION
The thermostat may be mounted to a wall surface or panel board using the two mounting holes provided in the back of the case. The desired mounting position is with the element bellows pointing down.
For accurate thermostat operation, the sensing element should be horizontally serpentined across the face of the coil to sense temperature in all areas.
Figure 1. Recommended mounting and sensing element installation.