Setup and adjustments - PENN Controls - A421ABG - A421AEJ - A421ABJ - Electronic Temperature Control - A421 Standard Model

A421 Series Standard Electronic Temperature Controls with Power Cords Installation Guide

Product
Controls > Temperature Controls > A421 Standard Model
Document type
Installation Guide
Document revision
E
Revision date
2022-08-25
Part number
24-7664-3027

The front panel of the A421 Series Electronic Temperature Control has an LCD and a three-button UI as shown in the following figure.

Figure 1. A421 Control front panel with LCD and three-button UI