Advanced menu - PENN Controls - A421ABG - A421ABJ - A421AEJ - Electronic Temperature Control - A421 Standard Model

A421 Series Standard Electronic Temperature Controls with Power Cords Installation Guide

Product
Controls > Temperature Controls > A421 Standard Model
Document type
Installation Guide
Document revision
E
Revision date
2022-08-25
Part number
24-7664-3027
You can use the Advanced menu to change the parameter values in the Basic menu and the parameter values for the following advanced parameter codes:
  • Temperature Units (Un)
  • Temperature Setback (tSb)
  • Sensor Offset (So)
  • High Temperature Setpoint Stop (HtS)
  • Low Temperature Setpoint Stop (LtS)
  • Backlight Level (bLL)

See Parameter codes and modes of operation and Table 1 for more information about parameter codes, usable parameter values, and default values.

Figure 1. Navigating the Advanced menu