Troubleshooting - PENN Controls - A421GBF - A421AEC - A421ABC - A421GEF - Electronic Temperature Control - A421 Standard Model

A421 Series Standard Electronic Temperature Controls Installation Guide

Product
Controls > Temperature Controls > A421 Standard Model
Document type
Installation Guide
Document revision
G
Revision date
2022-08-25
Part number
24-7664-3019

A421 Series Controls display fault codes on the LCD as described in the following table.

Table 1. Fault codes
Fault code Definition System status Solution
SF flashes alternately with OP Open temperature sensor or sensor wiring Output functions according to the selected SF mode See Troubleshooting procedure. Cycle power to reset the control.
SF flashes alternately with SH Shorted temperature sensor or sensor wiring Output functions according to the selected SF mode See Troubleshooting procedure. Cycle power to reset the control.
EE Program failure Output is off To reset the control, press MENU. If problems persist, replace the control.