Adjusting the control in Restricted mode - PENN Controls - A421GBF - A421AEC - A421ABC - A421GEF - Electronic Temperature Control - A421 Standard Model

A421 Series Standard Electronic Temperature Controls Installation Guide

Product
Controls > Temperature Controls > A421 Standard Model
Document revision
G
Revision date
2022-08-25
Part number
24-7664-3019

About this task

In this task you adjust the OFF value and shift the On and OFF control band within the restricted adjustment range, when the control is in the restricted adjustment mode.

Procedure

  1. On the Main screen, press MENU to go to the Restricted Adjustment mode menu and display the OFF parameter code screen (Figure 1).
  2. To go to the OFF value screen, press MENU again.
  3. On the OFF value screen, press Down or Up to change the OFF value within the restricted adjustment range.
  4. To save the selected OFF value and return to the OFF code screen, press MENU.
  5. To return to the Main screen, press Down or Up simultaneously.
    Figure 1. Adjusting temperature in the Restricted menu