About this task
In this task you access the Advanced menu and view and change the Advanced parameter values.
Procedure
-
On the Main screen, press and hold Down or
Up simultaneously for 5 seconds.
Undisplays on the LCD, which is the first parameter code screen displayed in the Advanced menu. - To scroll through all of the advanced parameter codes and display the preferred code, press Down or Up
- With the preferred parameter code displayed, press MENU to display the current parameter value for the code.
- With the current parameter value displayed, press Down or Up to scroll through all of the parameter code’s usable values and display the preferred value.
- With the preferred parameter value displayed, press MENU to save the displayed value and go to the next parameter code.