Use the Basic menu to quickly edit the On and OFF temperature values, as well as the Sensor Failure Mode (SF) and the Anti-Short Cycle Delay (ASd) value. See Parameter codes and modes of operation and Table 1 for more information about parameter codes, usable parameter values, and default values.
Note: Use the Up and Down arrows to navigate through the basic menu, to return to the main screen and to edit settings in the menu. Press the MENU tab to save settings in the basic menu.
Feature | Description |
---|---|
1 | Main screen |
2 | Basic menu |
OFF | Relay off temperature |
On | Relay on temperature |
SF | Anti-short cycle delay |
ASd | Sensor failure. 0= output relay de-energized. 1=output relay energized |